Skip to content
   

New Controller Platform Delivers Ease of Use for Latest Mobile Diesel Generator

By Generac PR Staff January 15, 2019

MDG25_3-4 BACK

Controller delivers high functionality with customers in mind

Generac Mobile’s MDG25 compact mobile diesel generator is ready to roll out the door with a new controller. The DeepSea 7310 puts the customer first. With less buttons, the controller is user friendly and it features an easy-to-read status screen. The new controller also boasts additional inputs and voltage settings.

The MDG25 offers the same great performance as the MMG25, but in a smaller and more serviceable package. This unit provides three-phase 25 kVA prime power in a compact cabinet. The cabinet design enables maximum space and transport efficiency while making the generator easy to maneuver and tow. The Final Tier 4 Isuzu engine is reliable and easy to maintain.

Designed with operator safety in mind, the MDG25 is loaded with features to enhance safety and security on the job. A recessed external E-Stop is easy to locate and access in emergencies. The unit also features access doors with auto shutdown that separates the main breaker access from load cables, automatically shutting down the unit if the lug door is open. The controller is also located on the rear of the unit away from power wires and service points and it is lockable for security and safety.

About Generac Mobile
Generac Mobile is a leading manufacturer of mobile light towers, generators, heaters and pumps. A wholly owned subsidiary of Generac Power Systems (NYSE: GNRC), Generac Mobile is headquartered in Berlin, Wis., where it manufactures all product lines to withstand the rigors of rental yards, commercial construction jobsites and extreme environments. The company’s innovative solutions help construction, infrastructure, military, disaster response, oil and gas, mining and event professionals optimize their operations with mobile light, power, water and heat solutions, providing safer worksites and streamlined workflows that maximize efficiency and profit. Visit www.generacmobileproducts.com for more information.

Related Article

New LED Light Tower Shines in the Extremes

MLT4060MVD_Mobile_Light_Tower

Engineering the next generation of light towers is all about delivering energy efficiency while ensuring maximum durability for demanding operating conditions. For those times when... Read More >