Skip to content
   

Generac Industrial Power Launches Largest Gaseous Generator Set Yet

By Generac PR Staff July 26, 2018

750kw

Company continues expansion into larger gaseous generators

Generac Industrial Power’s experience and innovative technological advances in natural gas generators continues with its latest generator set. The new 750 kW generator is the company’s largest and most powerful gaseous generator to date.

The 750 kW design features Generac’s new G33.9L engine, developed from a proven diesel block. It combines Generac’s long-standing spark-ignited engine expertise with the robust fuel delivery and ignition systems of Motortech, which Generac acquired in 2017. The G33.9L is designed to deliver a larger displacement engine platform with high power density, optimized to perform in various demanding power system applications while providing a strong value proposition and performance.

Available in both a single-set (SG750) and modular power system (MPS, MG750) configurations, the 750 kW unit is U.S. Environmental Protection Agency (EPA) certified for standby and demand-response applications. It is also available with EPA stationary non- emergency emissions certification.

The 750 kW generator features Generac’s new control panel platform, Power Zone®. The Generac Power Zone controller makes interaction with a generator more intuitive. The controller is the first industrial gen-set control platform on the market with built-in Wi-Fi, Bluetooth, LAN and Webserver, putting monitoring and control within reach of any mobile device or PC with internet connectivity. The Power Zone provides instant access to generator and engine parameters, ensuring the unit is ready and available at a moment’s notice. The controller also regulates the MPS paralleling configurations.

About Generac (NYSE:GNRC)
Generac Power Systems is a leading global supplier of backup power and prime power products, systems and engine-powered tools. Back in 1959, our founder was committed to designing, engineering and manufacturing the first affordable backup generator. Fifty-nine years later, the same dedication to innovation, durability and excellence has resulted in the company’s ability to expand its industry-leading product portfolio into homes and small businesses, on job sites, and in industrial and mobile applications across the globe. Generac offers single engine backup and prime power systems up to 2 MW and paralleled solutions up to 100 MW, and uses a variety of fuel sources to support power needs for our customers. We are proud to be named, in back-to- back years, the Frost & Sullivan 2014 and 2015 North American Natural Gas Generator Set Company of the Year. Visit GeneracIndustrialPower.com for more information.

Related Article

New Controller Platform Raises Bar on Connectivity, Ease of Use

PowerZoneFront

Power Zone delivers high functionality and unprecedented connectivity with smartphone-esque interface According to the Pew Research Center, a whopping 77 percent of Americans own smartphones.... Read More >