Skip to content
   

New LED Light Tower Shines in the Extremes

By Generac PR Staff March 1, 2017

MLT4060MVD_Mobile_Light_Tower

Engineering the next generation of light towers is all about delivering energy efficiency while ensuring maximum durability for demanding operating conditions. For those times when the mercury falls to bone-chilling levels or when the scorching heat sends others packing, Generac Mobile Products has a new lighting solution to keep the job site active: the MLT4060MVD light tower.

Engineered to deliver long-lasting lighting with minimum power consumption — making it ideal for the extreme or remote job site — the MLT4060MVD comes equipped with four Generac 240 W LED light fixtures and an extended-run ECOSpeed™ engine. The engine can be easily controlled, allowing it to operate on multiple speed settings that create better fuel efficiency, up to 580 hours of runtime, the ability to make adjustments during times when more or less light is needed.

The Generac Magnum Power Zone Autolight Controller features automatic start/stop and dusk-to-dawn photo sensor operation, making the light tower especially smart. A temperature management system is also built into the ECOSpeed™ engine design to keep the engine running smoothly while managing loads for days when the temperatures go as low as -40° F and as high as 120° F.

The four 240W LED light fixtures featured on the MLT4060MVD are waterproof, extremely durable and create energy efficient light that consumes minimal power. Deployed atop a mast with a maximum height of 23 ft., they have a combined total light output of 88,000 lumens and are warranted for 5 years or 10,000 hours of use.

“We built this light tower for those professionals who need light absolutely anywhere,” said Mark Hanson, vice president of sales, Generac Mobile Products. “Working on a job site in extreme conditions is tough, so we made this light tower as easy as possible to operate, re-fuel, and service and as tough as the professionals who use it.”

The MLT4060MVD light tower also offers a rust-resistant, powder-coated aluminum enclosure, 359 degree mast rotation and an extended 750-hour service interval.

About Generac Mobile Products

Generac Mobile Products is a leading manufacturer of mobile light towers, generators, heaters and pumps under the Generac®, Magnum® and Generac MAC® brands. A wholly owned subsidiary of Generac Power Systems (NYSE: GNRC), Generac Mobile Products is headquartered in Berlin, Wis., where it manufactures all product lines to withstand the rigors of rental yards, commercial construction jobsites and extreme environments. The company’s innovative solutions help construction, infrastructure, military, disaster response, oil and gas, mining and event professionals optimize their operations with mobile light, power, water and heat solutions, providing safer worksites and streamlined workflows that maximize efficiency and profit. Visit www.generacmobileproducts.com for more information.

Related Article

New Controller Platform Delivers Ease of Use for Latest Mobile Diesel Generator

MDG25_3-4 BACK

Controller delivers high functionality with customers in mind Generac Mobile’s MDG25 compact mobile diesel generator is ready to roll out the door with a new... Read More >